To first time users (help)
What is the Electric Actuator Selection System?…
The Electric Actuator Selection System is a WEB system that makes choosing products according to the customer's usage simple.
By just selecting the operating conditions, inputting the required values and the optimum combination of products will be selected for you.
Precautions when using 2 or more browsers simultaneously.
This system uses Cookies for recording the selection information. Therefore, if multiple browsers are used simultaneously, the capacity of the storage may be overwhelmed when making a selection, and proper operation may not be possible.
Whenever possible, please use only 1 browser during the operation.
System Conditions used
In order to properly use our System, the following environmental conditions indicated below will become necessary.
Browser conditions (Operation of the following browser versions have been confirmed.)
- Microsoft Internet Explorer 8.0 or above
- The newest versions to Chrome, Firefox, Safari, Opera, Edge and 1 version before.
- Others: HTML5 compatible browsers
Cookies are used
This system uses Cookies, and so be sure that the browser setting is such that Cookies are enabled.
JavaScript is used
This system uses JavaScript, and so be sure that the browser setting is such that JavaScript is enabled.
StyleSheet is used
This system uses a proprietary StyleSheet, and so be sure that the browser setting is such that StyleSheet is enabled.